Username Password SUBMIT Remember Me Sign up
Login
Enter Zip/Postal Code GO Outside the U.S. and Canada?
Logging in ...
BAC @ YOU

Latest Post

06 Apr

Alternate Materials of Construction

Hi my name is Kavita Vallabhaneni…that’s me in the Headquarters video.  I am the Manager of Product Marketing and now a blogger.  I’m excited about blogging as I’ve never blogged before so I wanted to come up with an interesting topic.  I didn’t think my obsession with reality TV would be note-worthy so I chose materials of construction.

There are several materials of construction available for evaporative cooling products.  The industry standard is Galvanized Steel.  Then there is the shiny, sleek stainless steel but it’s pricy as well.  Another is fiberglass reinforced polyester (FRP).

At BAC we like to think outside the box when it comes to corrosion resistant materials of construction.  I want to spend this time talking about the TriArmor® Corrosion Protection System.  We named it TriArmor® because it has three levels of protection for the cold water basin.  It consists of G-235 Galvanized  Steel substrate with a Thermosetting Hybrid Polymer and a proprietary Polyurethane Barrier sprayed on the inside of the basin after its been assembled.

We introduced the material after a decade of field and R&D testing.  BAC wanted to be assured that the material would last the life of a cooling tower.  So we ran it through a gamut of tests including, tension, shear, shock, chemical etc.  TriArmor® withstood all these tests with excellent results.  Another positive feature about TriArmor® is that it offers superior corrosion resistance compared to Type 304 and 316 stainless steel, but at a lower cost.

Next time, the story continues…who will win:  the new edgy TriArmor or the tried and true stainless steel?

« Post by HoweKool - Permalink »

Commenting on BAC @ You posts is one of the many benefits of becoming a member of The Loop, click here to register today.

Recent Posts

29 Mar
0 Comments

Resource Central

One of the great places on BAC’s website, in case you haven’t explored it, is [...]

21 Mar
0 Comments

Maintenance time!

A few of us here in Baltimore are greeting the beautiful spring weather by bringing [...]

07 Mar
1 Comments

Revit!

You’ve asked for it. And now you’ve got it! Revit content is now available for [...]