March 12th, 2009
BAC is pleased to announce that the Cooling Technology Institute (CTI) has certified the thermal performance of BAC’s FXV, VF1 and VFL Closed Circuit Cooling Towers with both ethylene and propylene glycol as the process fluid.
This is the first time the thermal performance of closed circuit cooling towers has been certified with fluids other than water by CTI!
For over 25 years BAC has led the evaporative cooling industry to require independent verification of thermal performance through the CTI Certification program. The value of having certified products is now widely recognized. Today, CTI has a total of 43 certified products that are manufactured by 18 different manufacturers. For more information on the growth of the certification program, visit http://www.cti.org/downloads/2008CertificationSpeech.pdf.