|
Our Technology
BAC products make use of the desirable properties of water,
one of nature's most abundant cooling media, to provide
cooling solutions for air conditioning, industrial processes,
power generation and refrigeration. In most areas of the
world, water is abundant and inexpensive, and its "latent
heat", or ability to reject or absorb large quantities of
heat through evaporation (latent heat of vaporization) or
freezing (latent heat of fusion) make it ideal for these
applications:
Evaporative Cooling:
BAC's cooling towers, closed-circuit cooling towers and evaporative
condensers make use of evaporative cooling. That is what
makes you feel cool when you climb out of a swimming pool
or the ocean on a breezy day. Evaporation from the water
on your skin pulls heat from your body and makes you feel
colder than the surrounding air. The same thing is true
in one of our evaporative cooling products. The evaporative
cooling principle makes it possible to cool or condense
to a lower temperature than simple dry-air cooling, so you
save on space, equipment cost, and energy consumption. No
wonder evaporative cooling is the first choice at most central
chiller plants and industrial cooling installations around
the world!
Ice Thermal Storage:
Ice thermal storage uses the latent heat of fusion of water
to "store" thermal energy as ice. The advantage of this
"thermal storage" is the fact that electrical energy can
be used during off-peak periods to provide cooling during
peak periods. In other words, the operator of an ice thermal
storage system can run chillers to generate cooling effect
during periods when energy is inexpensive (usually at night),
and use the ice to provide cooling for the building system
during the peak periods (usually during the day). This is
called "demand-shifting," and in many cases utilities will
provide economic incentives for owners to install ice thermal
storage systems to shift the electrical demand from peak
periods to off-peak periods.
In addition to savings from incentives and off-peak energy
consumption, other significant first cost advantages are
realized from thermal storage using ice. Cooling with ice
allows systems to operate with 36°F cooling water and
a cooling range up to 20°F, so piping and pump sizes
can be reduced compared with conventional systems. Designing
around low temperature air distribution means that ductwork
sizes can also be reduced.
Research and Development at BAC:
Research and development for BAC's evaporative cooling and
thermal storage products are conducted at BAC's 40,000 square
foot test facility in Jessup, MD, one of the most advanced
in the industry. Here, BAC engineers and technicians can
simulate the broad range of environmental and system operating
conditions encountered by our products in actual use. After
new concepts are screened by computer modeling, tests are
conducted on equipment ranging in size from small prototype
modules up through full-scale field-erected cooling towers.
In addition to thermal
testing in controlled-environment test chambers, a wide
range of material and component development activities are
conducted, including fan development, static and dynamic
stress evaluations, accelerated aging and corrosion testing,
hydraulic tests and wind tunnel tests. Dozens of patents
and a complete line of evaporative cooling and thermal storage
products have resulted from this state-of-the-art facility.
Since its founding
in 1938, Baltimore Aircoil Company has specialized in the
design and manufacture of evaporative cooling and heat transfer
equipment, and has become a world leader in this field.
BAC's continuing program of research and development has
produced many innovations which have evolved to become the
standards of the industry.
|