<?xml version="1.0" encoding="UTF-8"?>
<rss version="2.0"
	xmlns:content="http://purl.org/rss/1.0/modules/content/"
	xmlns:wfw="http://wellformedweb.org/CommentAPI/"
	xmlns:dc="http://purl.org/dc/elements/1.1/"
	xmlns:atom="http://www.w3.org/2005/Atom"
	xmlns:sy="http://purl.org/rss/1.0/modules/syndication/"
	xmlns:slash="http://purl.org/rss/1.0/modules/slash/"
	>

<channel>
	<title>Cooling Towers, Closed Circuit Cooling Towers, Evaporative Condensers, Aircoil Evaporators, Ice Thermal Storage Systems -- Baltimore Aircoil Company &#187; Industry Resources</title>
	<atom:link href="http://www.baltimoreaircoil.com/english/category/resource-types/industry-white-papers/feed" rel="self" type="application/rss+xml" />
	<link>http://www.baltimoreaircoil.com/english</link>
	<description>Baltimore Aircoil is a manufacturer of Cooling Towers, Closed Circuit Cooling Towers, Evaporative Condensers, Aircoil Evaporators, and Ice Thermal Storage Systems.</description>
	<lastBuildDate>Tue, 14 May 2013 21:08:02 +0000</lastBuildDate>
	<language>en</language>
	<sy:updatePeriod>hourly</sy:updatePeriod>
	<sy:updateFrequency>1</sy:updateFrequency>
	<generator>http://wordpress.org/?v=3.3.1</generator>
		<item>
		<title>Blue Waters</title>
		<link>http://www.baltimoreaircoil.com/english/13035/blue-waters</link>
		<comments>http://www.baltimoreaircoil.com/english/13035/blue-waters#comments</comments>
		<pubDate>Wed, 27 Jul 2011 15:06:27 +0000</pubDate>
		<dc:creator>HoweKool</dc:creator>
				<category><![CDATA[Blog]]></category>
		<category><![CDATA[Industry Resources]]></category>
		<category><![CDATA[Products]]></category>
		<category><![CDATA[Series 3000]]></category>

		<guid isPermaLink="false">http://baltimoreaircoil.com/english/?p=13035</guid>
		<description><![CDATA[In 2011, on the campus of the University of Illinois at Urbana-Champaign, a supercomputer of [...]]]></description>
			<content:encoded><![CDATA[<p>In 2011, on the campus of the University of Illinois at Urbana-Champaign, a supercomputer of unprecedented power will be unveiled by the National Center for Supercomputing Applications (NCSA) and it will be cooled by Series 3000 Cooling Towers. This IBM system named Blue Waters will be one of the top supercomputers in the world.</p>
<p>Supercomputers are typically cooled by air cooled systems. However, for IBM Power7 hardware, a water cooled system is used which is much more energy efficient. Blue Waters will be cooled by water that is being pumped through very small pipes running across its circuit boards, allowing the components to be closer together and cutting down on internal communication time. According to IBM, by using water cooling the energy requirements will be reduced by 40 percent when compared to traditional air-cooled systems. Additionally, the cooling towers will provide free cooling for approximately nine months of the year. Water alone is what enables Blue Waters to have its speed while also being energy efficient.</p>
<div id="attachment_13037" class="wp-caption alignnone" style="width: 241px"><a href="http://baltimoreaircoil.com/english/resource-library/file/1467"><img class="size-full wp-image-13037    " title="Blue-Waters-Cooling-Towers_web" src="http://baltimoreaircoil.com/english/wp-content/uploads/2011/07/Blue-Waters-Cooling-Towers_web.jpg" alt="Blue Waters Cooling Towers" width="231" height="154" /></a><p class="wp-caption-text">Blue Waters Cooling Towers - Photo Credit: NSCA</p></div>
<p>The cooling towers selected for this job were three 31056C Cooling Towers. Galvanized steel with upgraded stainless steel hot water basins and welded stainless steel cold water basins. These cooling towers run on belt drives for easy maintenance and compatibility with variable speed drives. Kent Reifsteck, Manager of Engineering Services for the University of Illinois at Urbana-Champaign estimates, “over the five year life span of the supercomputer, there will be $20 million saved in cooling costs because of these cooling towers.”</p>
<p>In addition to cooling the Blue Waters supercomputer, these cooling towers will also provide water to air-condition the building. The National Petascale Computing Facility will achieve LEED® Gold certification for energy efficiency, thanks in part to the cooling towers.</p>
<p>Ever seen  cooling towers look so pretty? Click on the picture or <a title="Blue Waters Article" href="http://baltimoreaircoil.com/english/resource-library/file/1467">click here</a> to link to an article reposted in our Knowledge Center written about the project by the University of Illinois Alumni magazine. We also have a great <a title="Blue Waters Project Report" href="http://www.baltimoreaircoil.com/english/resource-library/file/1469">project report in the Knowledge Center</a>!</p>
]]></content:encoded>
			<wfw:commentRss>http://www.baltimoreaircoil.com/english/13035/blue-waters/feed</wfw:commentRss>
		<slash:comments>0</slash:comments>
		</item>
	</channel>
</rss>