Home
About BAC
Products
Service
Markets Served
Careers
Resources
Find a Sales Rep
Contact Us
Products   
 


ICE CHILLER® Thermal Storage Products


Overview · Case Studies · Engineering Data · Modes of Operation · System Schematics · Benefits · Custom Coils · Application Guide · Specifications · Operation and Maintenance · Rigging and Assembly
Downloads: Brochures · Product Reports · Project Reports · CAD Drawings

Ice Chiller® Thermal Storage Product Benefits


Lowest First Cost
Systems with ice thermal storage can be installed at the same or lower first cost than traditional systems when designed with the colder supply water available from ice. The savings that result from the use of smaller chillers and cooling towers, reduced pump and pipe sizes and less connected horsepower, offset the cost of the ice thermal storage equipment. Additional savings can be found when using lower temperature air distribution, which allows reduced ductwork and fan sizes.

 
 

Smaller Chillers and Heat Rejection Equipment: By designing the system around 24-hour per day chiller operation, the size of the chillers and cooling towers or air-cooled condensers required for an ice system is significantly reduced, when compared to conventional chillers and heat rejection equipment sized for the instantaneous peak load. A typical thermal storage design includes chillers that provide 50 to 60% of the peak cooling load. The balance of the cooling requirement is provided from the ice storage system.

• Reduced Pump and Pipe Sizes: Pump and pipe sizes are also reduced in a properly designed ice storage system. Substantial savings in the chilled water distribution loop are realized when the system design incorporates reduced flow rates that result from using a larger temperature range in the water loop. Use of a larger temperature range, for example 18°F (10°C) instead of the more traditional 10°F (5.5°C) temperature range results in a reduction of pipe size. Condenser water pipe sizes are reduced due to lower flow requirements for the smaller chiller. Pump savings due to reduced chilled water and condenser water flow rates are also realized.

• Reduced Cooling Coil and Supply Air Fan Sizes: Cooling coils sized using lower supply water temperatures and traditional supply air temperatures are generally smaller due to fewer rows. the reduction in rows leads to lower supply fan HP (kW).

• Reduced Air Handling Equipment: When the air distribution is designed with lower supply air temperatures, the size of the ductwork, fans and fan motors are reduced.

• Reduced Electrical Distribution: Smaller chillers, heat rejection equipment and pumps require less horsepower than a traditional system, which results in smaller transformers, switchgear, wire sizes and starter panels.

• Reduced Generator Size: If a facility has a generator for daily or back-up power, the size of the generator will be significantly reduced when the peak electrical load of the facility is reduced using ice storage.

Reduced Energy Cost
An ice thermal storage system reduces peak demand, shifts energy usage to non-peak hours, saves energy, and reduces energy costs.

• Reduces Peak Demand and Shifts Energy Usage: With less connected horsepower, ice storage can lower peak electrical demand for the HVAC or process cooling system by 50% or more. Since most electrical rates include demand charges during peak demand times and/or higher day versus night kWh charges, savings on electrical bills can be substantial. Peak electrical demand rates of $15 to $18 per kW are not uncommon. In areas with “real time pricing”, where the electric rate varies hour by hour based on the market price of electricity, day to night kWh costs can vary by 500 to 1000%. The use of electricity at night versus peak daytime hours can lead to large savings on energy bills.

Saves Energy: In addition, total annual kilowatt-hours used are less when the system is designed taking advantage of the low supply water temperature available from the ice storage system. Lower kWh consumption is possible for five reasons:

1. Although making ice requires more energy than producing chilled water, the efficiency penalty is not as large since the ice is made at night when condensing temperatures are lower, increasing the efficiency of the chiller.

2. Ice systems typically operate the chiller at full load. Chillers are inefficient when run with low loads during the spring and fall. A typical chiller will operate at less than 30% capacity for half the year.

3. Reduced pumping horsepower.

4. Reduced fan horsepower due to lower air pressure drop across the cooling coil. A higher chilled water temperature differential across the cooling coil usually results in fewer rows and therefore a lower pressure drop.

5. The ability to recover waste heat from the chiller for heating water both night and day.

 
 

Additional kWh savings are possible if the air distribution is designed to take advantage of the low temperatures available from the ice storage system. As the electric industry continues to deregulate, and time-of-use rates, real time pricing schedules and negotiated power prices become standard, ice storage can provide even greater future savings in operating costs.

Variable Capacity
The ice thermal storage system will maintain a constant supply temperature regardless of the variations in instantaneous cooling demand. The flow and entering water temperature set the instantaneous capacity.

Improved System Reliability
Ice storage systems provide the reliability necessary to ensure air-conditioning is available. With traditional systems, installing multiple chillers provides redundancy. In the event of a mechanical failure of one chiller, the second chiller provides limited cooling capacity. The maximum available cooling for the traditional system would only be 50% on a design day.

Most ice storage systems utilize two chillers in addition to the ice storage equipment. Two chillers are designed to provide approximately 60% of the required cooling on a design day while the ice storage provides the remaining 40% of the cooling capacity. In the event only one chiller is available to provide cooling during the day, up to 70% of the cooling capacity is available. The one operable chiller provides 30% of the cooling requirement while the ice rovides up to 40%. Based on typical HVAC load profiles and ASHRAE weather data, 70% of the cooling capacity would meet the total daily cooling requirements 85% of the time.

Reduced Maintenance
The ice thermal storage coils have no moving parts so very little maintenance is required. Because the chillers, pumps and heat rejection equipment are smaller, ice storage systems will have less maintenance than a traditional system. The ice thermal storage system also allows a chiller to undergo routine maintenance during the day when the ice storage can handle the system load.

Environmentally Friendly
Reducing energy consumption and using electricity at night will reduce global warming. Electricity generated at night generally has a lower heat rate (lower fuel use per power output), and therefore lower carbon dioxide and greenhouse gas emissions resulting in less global warming. The California Energy Commission concluded that the use of electricity at night created a 31% reduction in air emissions over the use of electricity during the day.

With smaller chillers, an ice thermal storage system reduces the amount of refrigerant in a system. Most refrigerants in use today are slated to be banned in the future under the Montreal Protocol because they contribute to global warming. Using smaller amounts of refrigerant helps to save the ozone and reduce global warming.

One of the Amsted Industries

| Home | About BAC | Products | Markets Served | Employment |
| Resources | Find a Sales Rep | News | Events | Privacy Policy | Contact Us |